Hi All...
I'm using both the FaxLib and VoLib components in my project. I'm using the following versions respectively:
faxlib_C55_CPU3_2_1_0_1 and volib_C55_CPU3_2_1_0_1.
I see that there are some component folders like "util" which is present in both these FaxLib and VoLib folders. On inspection both the folders libraries are different. So which one to use in our project..?
Should I use both..?
Please guide me.
Thanks & regards,
Ashok