Hi
in "TMS320C5515/14/05/04/VC05/VC04 DSPGeneral-Purpose Input/Output (GPIO) User's Guide"
it is said:
"When an interrupt occurs on an enabled GPIO pin, the GPIO interrupt flag registers (IOINTFLG1 and IOINTFLG2) latch the corresponding bit to a "1". The interrupt signal to the CPU will be kept low until all flag bits in the IOINTFLG1 and IOINTFLG2 registers are cleared"
what happens if during gpio ISR, triggered by one GPIO, another flag (of a different GPIO) is raised (and is not cleared upon exiting the ISR).
will I get another interrupt? Or am I stuck till I clear the second bit raised?
thanks
Yaron