Hi Everyone,
I have got a typical question here for you.
I am using Arduino which is then connected to DSP c5515 usb stick. I am using code composer 5.0 version to connect the code through Arduino to the DSP. Initially i have performed some UART tests to conclude that something was working and was successful in getting the echo back to the console.
Now i want to test the tone(sound). Am using aic3204 to do that. but i want DSP to identify the inputs given by me and then play a tone simultaneously.
Do I need to connect(combine) 2 projects to get the desired result?
Note: I know that i can use just DSP by itself for the tests. But for some reason my DSP seems not responding well. Hence i started using Arduino using the Serial IO with C coding thru Arduino. Now i want to do the same thing for the Tone recognition.