We have a custom board utilizing a C5533 DSP. I am using Code Composer 5.4 to build and debug the application. That works well. We are not at a point where the code needs to be placed into SPI flash from which the DSP will boot. We are using a micron M25P10 device to store the code. I have programmed the flash device with the executable which has been converted from the *.out file to a bin file. I have Code Composer 5.4 executing a post build step :
hex55 -i app.out -o app.bin -b -serial8 -boot -v5505
which builds the boot image. The produced app.bin is then burned into the flash, the custom board is reset and ....... nothing. Am I missing something. The same code runs well when debugged using Code Composer and Olimex TMS320-Jtag-XDS100-V2 device.