Hello!
Suddenly I have a problem on my custom board. The board contains TMS5509A and parallel flash M28F320 connected to EMIF. Boot pins are configured to boot through EMIF (1011). Although board contains special chip that holds processor in reset for about 200 ms after power on.
But when I try to connect to the target using XDS100 and CCS 5.5 emulator I get an error:
The core is hanged
If I change boot pins configuration on anything else, core is working properly and I can debug.. I can work with flash during debugging, and it is working correctly - it can be programmed and erased..
So where can be the problem, than the core is hanged and can not be booted from parallel flash?
Regards,
Alex