Hello,
I'm trying to get simple DSPLIB functions to work in my application, specifically the fir2 function. The problem is that whenever I call it, my program halts. I don't know why it's stopping, it just stops dead right when it calls the fir2 function. I guess I'm not very experienced with the DSK, so I don't know if this is what a segmentation fault looks like or not.
Here is what I've tried so far:
* I rebuilt dsplib specifically for the large memory model and my cpu revision (2.1)
* I made sure my coefficients and delay buffer were in internal memory, as per the dsplib reference manual.
* I tried building and running the examples, but the emulator fails when I try to load them (I can post the error message later).
Does anyone know what could be happening here? I found one other post from someone with my same issue, but there was no solution posted. My instinct tells me it's something with my variable allocation or memory map, because the dsplib code should just work. I'll keep plugging away at it, but please I've put a lot of time into this already and I'd like some help!
Thanks,
George