Hi,
I had a clock jitter problem on C5517 McBSP.
I measured the clock out pin and found the clock phase noise was worse than clock in.
How can I improve the clock jitter?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I had a clock jitter problem on C5517 McBSP.
I measured the clock out pin and found the clock phase noise was worse than clock in.
How can I improve the clock jitter?
You can probably clean it up by changing the PLL settings.
Let us know which clock pin you are measuring.
Also let us know your PLL and pin configurations (clock frequency and register values) from input to pre divider clock to post divider(s) to clockout sel.
Hope this helps,
Mark
The input clk is 16.384MHz to C5517 and the PLL settings lists below.
MOV #0101111100000000b, port(#PMR) ; PLL mult = (0x5F00 / 256) + 1 = 96
MOV #0000000000000011b, port(#PICR) ; PLL reference divider = 4, 16.384MHz / 4 = 4.096Mhz Ref freq
MOV #0000000000000000b, port(#PODCR); Output divider = 0 (OD = 0 + 1 = 1, OD2 = (0 + 1) * 2 = 2, OUTDIV2BY = 0)
MOV #0000000000000000b, port(#PCR) ; Normal operating mode
After that, I generated the 8.192MHz from McBSP_CLKX and found the phase noise was bad.
So, I measured C5517 General Purpose EVM's CLKOUT on HEADER3 to check it hardware or software issue.
http://support.spectrumdigital.com/boards/evm5517/revf/
I didn't happen this issue before when using 5409,5506 and 5507.
It looks like internal PLL design was modified on 5515 and 5517.
Hi All
I have some problem.
I use C5517-EVM with McBSP_Master_AIC3204_48kbps_POLL
I captured the waveform of McBSP_CLKX (L10) as below.
How can I improve the clock jitter?
From:
TMS320VC55XCSL-LOWPWR 03_04_00_02 :
C:\c55_lp\c55_csl_3.04\c55xx_csl\ccs_v5.0_examples\mcbsp\McBSP_Master_AIC3204_48kbps_POLL
By Will