A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am trying to optimize my power consumption on a board using the C5535. Right now I have the following configuration:
CLK_SEL = 1 (CLK_IN = 12 MHz with on board oscillator).
RTCX1 and X0 tied to on board 32 KHz crystal oscillator.
My concern is that in RTC Only mode, I would like to power off my oscillator to decrease power consumption in sleep mode.
Using Wake_up pin, I am able to switch from RTC only mode to active mode, but in active mode, I need the oscillator that has been set in sleep mode when entering in RTC Only mode.
So I am in a race condition where the DSP has to power off the oscillator, bu need it to wake up and run ...
Any idea about the way to manage RTC Mode, oscillator and crystal ?
Thanks.
Nicolas
As described in Power Configurations table in TRM, RTC clock must be running for RTC only mode. It can be turned off only when it is not used. In RTC only mode, it is used.
Regards.
I know about this.
My setup is the following :
* in RTC Only mode, C5535 is running using its 32.768 KHz crystal : OK
* in active mode, C5535 must be running from its CLKIn with a 12 MHz oscillator.
In order to reduce power consumption, in RTC only mode, I would like the DSP to put the external 12 MHz oscillator to be in sleep mode.
Switching from RTC only mode to active mode with the Wake up pin, DSP should power on the 12 MHz oscillator before, but It can't since it is in RTC only mode.
As a conclusion, trying to keep power consumption putting the external 12 MHz oscillator in sleep mode, the DSP will never be able to wake-up.
I have double checked : CLK_sel pin is not allowed to change during device operation; it must be tied high or low at the board.
Well, I think of this as similiar to the "chicken and egg" thing. Thus we have to have certain assumption which is clocked by the 32k RTC osc. It is low power and can be used to generate the higher operational clock frequency for the device via PLL. When going to RTC only mode, we shut off the PLL and all possible power to achieve a low power state. When waken up, the device activates DSP_LDO to bring up the system.
Regards.
The issue is that I use the DSP with a codec (AIC3204), and I have to be sure that both are using the same ref clk. Note that Codec is in Master mode.
If the DSP use the 32.768 crystal and the codec the 12 MHz oscillator, I know that my I²S data between DSP and Codec will be fine, but my other software framework won't work.
As a conclusion, the DSP must use the 12 MHz ref clk, not the 32.768 KHz crystal. But I also need to switch off the oscillator when the DSP in RTC Only mode ...
So yes, this is a kind of Chicken/egg/race condition.
Any idea ?
Note that BCLK=8 Ksps and BCLK=2x8x16=256 KHz.
Some other information regarding DSP PLL configuration:
// Use the 32.768 kHz internal clock
PLL_Config pllCfg_98MHz = {0x8BB4, 0x8000, 0x0806, 0x0000}; /* Ratio 2996 + 4 */
// Use the 12 MHz reference clock
// Nominal Frequency = 98.304 MHz = (12.0 MHz/125) * 1024
// Multiplier M = 1020 + 4
// Reference divider N = 121 + 4
PLL_Config pllCfg_98MHz = {0x83FC, 0x0079, 0x0806, 0x0000};
So I wonder if using the 32.768 KHz crystal, I can have both the PLL at 98.304 MHz and I²S at 8Ksps with BCLK at 256 KHz (16 bits legnth). I can perhaps check if I²S BCLK to be 16, 20, 24 or 32 bits to fit this condition. In that hypothesis, WCLK is still 8Ksps, but BCLK is
16 word length: 256 KHz
20 word length: 320 KHz
24 word length: 384 KHz
32 word length: 512 KHz
If you find a clock configuration for both DSP (98.304 MHz) and Codec (8Ksps) from 32.768 Crystal, so I will be able to remove 12 MHz ref clock.
I have found in datasheet that with 92.304 MHz sys clcok, it is impossible to have a 8KHz WCLK (WCLK=SYSCLK/2^(DIV+1)).
I will check if I can drive the codec from a 32.768 Khz freq and rather use Codec PLL to generate 8KHz from 32.768 KHz (multiplier is 4096)