Hi,
I've got a project where I am using the AIC3204 codec to stream audio data on the 5515 usbstk board, everything works fine in debug mode (in code composer v4). I've written a test project that flashes an LED, sends some UART data then reads from the codec and writes to the codec which works in debug mode, I've got everything commented out in the gel file and am doing all the initialization steps in the main code.
However, when I convert the .out file to a .bin and program the device it will hang when trying to do an AIC read. Everything else will work in standalone mode, flashing LEDs and using the UART pins, just not the codec.
Has anyone actually had the board working in standalone using the AIC3204_codec_read() codec?
Thanks in advance for any help,
James