Dear sir,
I am trying to program 2 timers (timer0 and timer1) to generate interrupts every 100us and 400us.
I have attached my program please look into it.
Problem is that both timer flags (T0FLAG & T1FLAG of TIAFR) are getting set every time control comes to ISR. below is the ISR.
#define REG_TIAFR *(volatile ioport Uint16*) (0x1c14)
#define TIM_TIAFR_TIM0_FLAG (0x0001u)
#define TIM_TIAFR_TIM1_FLAG (0x0002u)
volatile Uint16 temp = 0;
volatile Uint16 count = 0;
interrupt void gptIsr(void)
{
IRQ_clear(TINT_EVENT);
temp = REG_TIAFR;
if ( temp & TIM_TIAFR_TIM0_FLAG)
{
/* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */
REG_TIAFR |= TIM_TIAFR_TIM0_FLAG;
count++;
}
if (temp & TIM_TIAFR_TIM1_FLAG)
{
/* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */
REG_TIAFR |= TIM_TIAFR_TIM1_FLAG;
count =0;
}
EZDSP5535_LED_on(1);
/* Enable CPU Interrupts */
IRQ_globalEnable();
}
What part i am doing wrong, I don't understand. According to timer periods, count value should increase to 4 and then get reset to 0. This is not happening, every time the control comes into the interrupt T1FLAG is also getting set along with T0FLAG. My requirement is to raise T1FLAG with T0FLAG once in four times. I have filled the period values accordingly.
When i debug the code all the values in timer registers are changing properly, but system control register TIAFR is always getting set to 0x0003.
I have attached the complete program as main.c file.
Please tell me if there is anything missing or wrong in the program.
Thanks & Regards,
Raghu K
/* ============================================================================ * Copyright (c) Texas Instruments Inc 2002, 2003, 2004, 2005, 2008 * * Use of this software is controlled by the terms and conditions found in the * license agreement under which this software has been supplied. * ============================================================================ */ /** @file csl_gpt_example.c * * @brief Example test code to verify the CSL GPT module functionality * * \page page4 GPT EXAMPLE DOCUMENTATION * * \section GPT GPT EXAMPLE * * \subsection GPTx TEST DESCRIPTION: * This test code verifies the functionality of the CSL GPT (General * Purpose Timer) module. GPT module of C5505/C5515 DSP is used to provide * interrupts to the CPU to schedule periodic tasks or a delayed task. * GPT can be configured with a counter and pre-scaler divider value. When the * GPT is started counter will be decremented to 0. The rate at which this * count happens can be controlled by the prescaler divider value. GPT clock * is derived by dividing the CPU clock with the pre-scaler divider value. * * This test is having two parts. First part of the test verifies whether the * GTP is decrementing the counter or not. GPT is configured with a count value * 0xFFFF and pre-scaler divider value 256. GPT is started and counter value is * read. After few cycles of delay GPT counter value is read again. Both the * counter values are compared to verify whether the second count value is less * than the first counter value or not. * * During second part of the test timer count rate of the GPT is verified. * As the GPT clock is derived from the CPU clock based on the pre-scaler * value it possible to verify the GPT rate with respect to CPU clock rate. * GPT pre-scaler value is set to divide by 4. So the counter runs at a speed * that is 1/4th of the CPU clock. Clock at which the CPU is running during the * test is calculated using the function getSysClk(). This function returns * the value of system clock in KHz. Value of the system clock in KHz * represents the CPU clock cycles for one millisecond. GPT count value is set * to 1/4th of the CPU clock cycles for one millisecond. With this setup GPT * should take one millisecond to count down the counter value to 0. In other * way clock cycles executed by the CPU from the time GPT is started to the * time counter value reaches 0 should be equal to the number of cycles that * are executed by the CPU in one millisecond.GPT is configured to generate * interrupt when the count value reaches to 0. GPT is started and the CPU * clock cycles are counted in while loop. This loop increments a global * variable 'cpuCycleCount' until the GPT generate time-out interrupt. * This while loop execution is taking 12 CPU cycles. So the total CPU cycles * executed will be 12*cpuCycleCount. At the end of the test this CPU cycles * calculated are compared with the CPU clock cycles that will be executed in * one millisecond. The calculated CPU cycles can vary �1% from the actual * CPU cycles. If this condition is satisfied GPT is running at the configured * rate. * * NOTE: THIS TEST HAS BEEN DEVELOPED TO WORK WITH CHIP VERSIONS C5505 AND * C5515. MAKE SURE THAT PROPER CHIP VERSION MACRO IS DEFINED IN THE FILE * c55xx_csl\inc\csl_general.h. * * \subsection GPTy TEST PROCEDURE: * @li Open the CCS and connect the target (C5505/C5515 EVM) * @li Open the project "CSL_GPTExampale_Out.pjt" and build it * @li Load the program on to the target * @li Set the PLL frequency to 12.288MHz * @li Run the program and observe the test result * @li Repeat the test at PLL frequencies 40, 60, 75 and 100MHz * @li Repeat the test in Release mode * * \subsection GPTz TEST RESULT: * @li All the CSL APIs should return success * @li Timer count value comparison should be successful in the first part of * the test * @li Timer should run at the configured rate in the second part of the test * * */ /* ============================================================================ * Revision History * ================ * 05-Oct-2008 Created * ============================================================================ */ #include <stdio.h> #include "csl_gpt.h" #include "csl_intc.h" #include <csl_general.h> #include "ezdsp5535.h" #include "ezdsp5535_led.h" #define CSL_TEST_FAILED (1u) #define CSL_TEST_PASSED (0) #define CSL_PLL_DIV_000 (0) #define CSL_PLL_DIV_001 (1u) #define CSL_PLL_DIV_002 (2u) #define CSL_PLL_DIV_003 (3u) #define CSL_PLL_DIV_004 (4u) #define CSL_PLL_DIV_005 (5u) #define CSL_PLL_DIV_006 (6u) #define CSL_PLL_DIV_007 (7u) #define REG_TIAFR *(volatile ioport Uint16*) (0x1c14) #define TIM_TIAFR_TIM0_FLAG (0x0001u) #define TIM_TIAFR_TIM1_FLAG (0x0002u) #define CSL_PLL_CLOCKIN (32768u) extern void VECSTART(void); volatile Uint16 temp = 0; volatile Uint16 count = 0; volatile int i; /** * \brief GPT Count Read Test function * * This is function verifies reading the counter values from the GPT * * \param none * * \return CSL_TEST_PASSED - Success * CSL_TEST_FAILED - Failure */ Int16 CSL_gptCountReadTest(void); /** * \brief GPT Count Rate Verification test function * * This function verifies whether timer is running at the configured * rate or not. This function configures and enables the GPT interrupts * to indicate the expiry of the timer count. Test counts number of * cycles executed by the CPU after starting the timer till the expiry * of the timer. These cycles are used to verify the WDT count rate. * It is assumed that calculated CPU cycles will be with in the range * �1% actual CPU clock cycles. Test will be successful if the calculated * CPU cycles fall with in this range. * * NOTE: Changing the PLL setting in the middle (After getSysClk() call) * of the test will result in test failure. * * \param none * * \return CSL_TEST_PASSED - Success * CSL_TEST_FAILED - Failure */ Int16 CSL_gptIntrTest(void); /** * \brief Function to calculate the system clock * * \param none * * \return System clock value in KHz * */ Int16 CSL_gpt0InteruptEvery100MicroSeconds(void); /** * \brief Function to generate interupt at every 100us * * \param none * * \return System clock value in KHz * */ Uint32 getSysClk(void); /** * \brief GPT Interrupt Service Routine * * \param none * * \return none */ interrupt void gptIsr(void); /** * \brief main function * * This function calls the GPT test function and displays the * test result. * * \param none * * \return none */ /////INSTRUMENTATION FOR BATCH TESTING -- Part 1 -- ///// Define PaSs_StAtE variable for catching errors as program executes. ///// Define PaSs flag for holding final pass/fail result at program completion. volatile Int16 PaSs_StAtE = 0x0001; // Init to 1. Reset to 0 at any monitored execution error. volatile Int16 PaSs = 0x0000; // Init to 0. Updated later with PaSs_StAtE when and if ///// program flow reaches expected exit point(s). ///// void main(void) { Int16 result; Int16 i; EZDSP5535_LED_init( ); CSL_FINST(CSL_SYSCTRL_REGS->EBSR, SYS_EBSR_SP1MODE, MODE1); EZDSP5535_GPIO_init(); EZDSP5535_LED_off( 1 ); // Turn on user LED i EZDSP5535_LED_off( 3 ); printf("CSL GPT TESTS!\n\n"); /////INSTRUMENTATION FOR BATCH TESTING -- Part 3 -- ///// At program exit, copy "PaSs_StAtE" into "PaSs". PaSs = PaSs_StAtE; //If flow gets here, override PaSs' initial 0 with ///// // pass/fail value determined during program execution. ///// Note: Program should next exit to C$$EXIT and halt, where DSS, under ///// control of a host PC script, will read and record the PaSs' value. ///// result = CSL_gpt0InteruptEvery100MicroSeconds(); if(CSL_TEST_FAILED == result) { printf("TIMER IS NOT GENERATING INTERUPT EVERY 100us!!\n"); /////INSTRUMENTATION FOR BATCH TESTING -- Part 2 -- ///// Reseting PaSs_StAtE to 0 if error detected here. PaSs_StAtE = 0x0000; // Was intialized to 1 at declaration. ///// } else { printf("TIMER IS NOT GENERATING INTERUPT EVERY 100us!!\n"); } for(;;) { EZDSP5535_LED_on( 3 ); for (i=0; i<10000;i++); EZDSP5535_LED_off( 3 ); for (i=0; i<10000;i++); } } /** * \brief GPT Interupt generation function @100us * * \param none * * \return CSL_TEST_PASSED - Success * CSL_TEST_FAILED - Failure */ Int16 CSL_gpt0InteruptEvery100MicroSeconds(void) { CSL_Handle hGpt0; CSL_Handle hGpt1; CSL_Status status; CSL_Config hwConfig0; CSL_Config hwConfig1; CSL_GptObj gptObj0; CSL_GptObj gptObj1; CSL_TimRegsOvly regPtr0; CSL_TimRegsOvly regPtr1; status = 0; /* Open the CSL GPT0 module */ hGpt0 = GPT_open (GPT_0, &gptObj0, &status); if((NULL == hGpt0) || (CSL_SOK != status)) { printf("GPT0 Open Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT0 Open Successful\n"); } /* Open the CSL GPT1 module */ hGpt1 = GPT_open (GPT_1, &gptObj1, &status); if((NULL == hGpt1) || (CSL_SOK != status)) { printf("GPT1 Open Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT1 Open Successful\n"); } /* Reset the GPT0 module */ status = GPT_reset(hGpt0); if(CSL_SOK != status) { printf("GPT0 Reset Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT0 Reset Successful\n"); } /* Reset the GPT1 module */ status = GPT_reset(hGpt1); if(CSL_SOK != status) { printf("GPT1 Reset Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT1 Reset Successful\n"); } /* Disable the CPU interrupts */ IRQ_globalDisable(); /* Clear any pending interrupts */ IRQ_clearAll(); /* Disable all the interrupts */ IRQ_disableAll(); IRQ_setVecs((Uint32)(&VECSTART)); IRQ_plug(TINT_EVENT, &gptIsr); IRQ_enable(TINT_EVENT); hwConfig0.autoLoad = GPT_AUTO_ENABLE; hwConfig0.ctrlTim = GPT_TIMER_ENABLE; hwConfig0.preScaleDiv = GPT_PRE_SC_DIV_1; hwConfig0.prdLow = 2500; // timer count to generate interrupt every 100us hwConfig0.prdHigh = 0x0000; /* Configure the GPT module */ status = GPT_config(hGpt0, &hwConfig0); if(CSL_SOK != status) { printf("GPT0 Config Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT0 Config Successful\n"); } hwConfig1.autoLoad = GPT_AUTO_ENABLE; hwConfig1.ctrlTim = GPT_TIMER_ENABLE; hwConfig1.preScaleDiv = GPT_PRE_SC_DIV_1; hwConfig1.prdLow = 10000; // timer count to generate interrupt every 100us hwConfig1.prdHigh = 0x0000; /* Configure the GPT module */ status = GPT_config(hGpt1, &hwConfig1); if(CSL_SOK != status) { printf("GPT1 Config Failed\n"); return (CSL_TEST_FAILED); } else { printf("GPT1 Config Successful\n"); } /* Enable CPU Interrupts */ IRQ_globalEnable(); CSL_SYSCTRL_REGS->TIAFR = CSL_IAFR_TIMER_FLAG_0_1_2_RESETVAL; regPtr0 = hGpt0->regs; regPtr1 = hGpt1->regs; if ((regPtr0->TIMPRD1) == (regPtr1->TIMPRD1)) printf("Both Timer period values are configured to same count\n"); /* Start the Timers */ GPT_start(hGpt0); GPT_start(hGpt1); /* Wait for the timer interrupt */ return (CSL_TEST_PASSED); } interrupt void gptIsr(void) { IRQ_clear(TINT_EVENT); temp = REG_TIAFR; if ( temp & TIM_TIAFR_TIM0_FLAG) { /* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */ REG_TIAFR |= TIM_TIAFR_TIM0_FLAG; count++; } if (temp & TIM_TIAFR_TIM1_FLAG) { /* Clear Timer Interrupt Aggregation Flag Register (TIAFR) */ REG_TIAFR |= TIM_TIAFR_TIM1_FLAG; count =0; } EZDSP5535_LED_on(1); /* Enable CPU Interrupts */ IRQ_globalEnable(); }