Hi there,
Boards: EVM5515 and EzDSP5535
AER: aer_c55l_cpuv3.3_obj_17_0_0_0_Win32
CCS: 5.5
I am trying to evaluate AER demo project. It compiles but when I run that it always gets stuck. The last message in the console is Start data processing...
I looked through the code and identified that it never goes out from the function aerSimFread(). Inside of the function is numRead = fread(tempIoBuf, buf_size,
AERSIM_FIO_SIZEOF_WORD, file); So it reads two times and that gets stuck.
How it can be fixed?
Thanks.