I'm using C5501 and want to boot it through I2C-EEPROM(atmel), but dont't know how to program EEPROM.
Can I use DSP simulator and CCS5.5 to implement the work ?
Thanks for any help you can provide.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This is a legacy device, looks like there is no boot image programmer available in c5501 CSL example package.But in my understanding you could use the boot programmer programmer file available for C5515/35/17 device, and modify it (need to change the I2C address) to make it work for C5501.
C5515 CSL example package is available in the link http://www.ti.com/tool/sprc133 - download & install C55XCSL-LOWPOWER package & look for programmer example in specified path <>c55_lp\c55_csl_3.04\c55xx_csl\ccs_v5.0_examples\programmer.
Hope the above information helps.
Regards
Vasanth