Hi community member,
Please let me confirm the TRM description.
I found the following explanation on RTC-only mode in TRM.
> In addition, the RTC is able to output an alarm or periodic interrupt on the WAKEUP pin to cause external power management to re-enable power to the DSP core and I/O.
It seems that the Wakeup pin can use to re-enable the external power management IC. If customer system use the wakeup pin as Wake-up source from RTC-only mode, can this pin also use to re-enable external power management IC?
If yes, would you show us the schematics in order to use the Wake-up pin as wake-up interrupt and wake-up source for external power management IC?
If you have any question, please let me know.
Best regards.
Kaka