Hi, i can't make the pll start correctly.
I try mesure it with the audio interrupt that appen @ 48khz and using the clock counting tools in CCS
But i can't get more than 90 clock count on each interrupt wich mean that i m running @ 12mHZ
Ive try to put the SW3 pin1 on the dual position but without succes.
Here is the return i have from consol:
PLL frequency 100 MHz
REGISTER --- CONFIG VALUES
PLL_CNTRL1 82fa --- 82fa
PLL_CNTRL2 080e --- 0806 Test Lock Mon will get set after PLL is up
PLL_CNTRL3 8000 --- 8000
PLL_CNTRL4 0000 --- 0000
Any feedback would be much appreciate
Regards.