Hello,I'm beggining using my DSP and I've been looking for a way to perform the FFT in my TMSC5535 and Code Compsoer 4,but no one gives any good and clear example of how to use it. I tried this many ways of perform fft without any succes:
-I tried using the dsplib and the CFFT files included on it,but Code Composer throws me a lot of errors when trying to build the project.
-I tried using the hwafft mentioned in the sprabb6b file, but when I build the code,Code Composer don't recognize the functions "hwafft_br","hwafft_1024pts",it doesn't even recognize the Uint,Int32,etc. ,and nobody in the forums tells me where to find the fft library.
-I tried using breakpoints to export the data to Matlab so I can execute the fft there,but the breakpoints/watchpoints are drastically slowing down my program, so it's not the right choice.
-I tried using any cooley tukey algorithm to compute the fft but is the same case as the first, Code Composer simply doesn't build,throwing back a lot of errors.
I hope someone could help me with a well-explained example.