Hello,
I'm designing a device where in I have used TMS320C5515 DSP with 24-Bit SPI Flash to store my application program and a 64 Mb mSDRAM. My question is, to add Over The Air firmware upgrade feature to this device, is it possible to have a secondary Bootloader which will be able to boot my device and upgrade the firmware by over writing the application in the SPI flash.
If the above method is not a solution, can you tell me how can this be done?
Regards,
Supreeth