Hi,
I'm new to the DSP and all those embedded system stuff. I searched through the internet for answer, but didn't come across a satisfying one.
I was told to use a TMS320C5515 eZdsp USB Stick and a SimpleLink Wi-Fi CC3000 Evaluation Module in my project. My concern is:
The C5515 eZdsp has an I2S interface on connectors P1,P2 and the CC3000 has a SPI interface on headers J1,J2. I was told to just simply connect those two devices with these connectors. Is it going to work ? Or is there any way to reprogram the pins on C5515 and change I2S to SPI ?
There is also a chance that I've mistaken almost everything...and I'm totally wrong.
Thanks in advance,
Marcin