Hello out there,
I try to do a real time audiospectrum analyse with the TMS320 C5505 USB-STick.
i want to use the TMS320 for sound generation and for the CFFT and send the result of the Cfft to another imx6 board.
I try do generate different sounds like a Frequenzysweep from 20Hz to 20kHz.
So far the fft code is working, But i have some timing issues if i generate some sinus or other sounds.
Please, is someone out there to help me.
first time for me to work on a DSP.
Thank you
Korbi