Hi TI Experts,
Please let me confirm the following question.
[Question]
My customer said that the output binary file by hex conversion utility was not 16bits unit. The file size is 8753 bytes. If use this image, it seems that it worked. However, they would like to know whether there is any problem for operation even though the bin file was not 16bits unit. If add the pad byte to this, would you teach me that values?
I attached the part of map file as below.
*************
********************************************************************************
TMS320C55x Hex Converter v4.3.2
********************************************************************************
INPUT FILE NAME: <xxx.out>
OUTPUT FORMAT: Binary
PHYSICAL MEMORY PARAMETERS
Default data width : 8
Default memory width : 8
Default output width : 8
OUTPUT TRANSLATION MAP
--------------------------------------------------------------------------------
00000200..00003fff Page=0 Memory Width=8 ROM Width=16 "ROM1"
--------------------------------------------------------------------------------
OUTPUT FILES: xxx.bin [b0..b15]
CONTENTS: 00000200..000002ff vectors
00000300..0000030f main_prog0
00000310..000009f3 coef_rom
000009f4..00001d32 main_prog
00001d33..00002430 init_prog
*************
Or would you please check whether there is any problem for this binary? If you can check, I will send the .out , .mxp file, .bin, cmd files to you on offline. So please teach me your Email address.
If you have any questions, please let me know.
Best regards.
Kaka