Hi TI Experts,
Please let me confirm the following question.
[Question]
Now my customer use the boot image(binary file) size of odd byte sizes and using the HPI boot for their application. If use this image for C5503 with using the HPI boot, there will be a lack in 1 byte data because the HPI peripheral is 16 bit access.
So, would you please teach me the last "1byte" data value which my customer should send to C5503?
They checked the data size of binary file on file properties on Windows PC. And this size is 8753 bytes. So, the bit value is "70024" bits and the time of access is"4376.5". I would like to know the value of 8bit(1byte) data.
I do not know that the binary image size is depends on the boot file size(odd, even byte size). Is this influence on the access via HPI?
If you have any question, please let me know.
Best regards.
Kaka