Can I get the source code of ASRC(sample rate converter) on C55 connected audio framework.
The library of ASRC (asrc_dly_fix_lib.lib) on current "connected audio framework" is build for C55x CPU Rev 3.x.
But I want to use this framework with other libraries built for CPU Re v2.X.
Now I got an error :
asrc_dly_fix_lib.lib<asrc_dly_fix.ob
j>" specifies "C55x CPU Rev 3.x", which is not compatible with "C55x CPU Rev
2.x" specified in a previous file or on the command line
So I want to build ASRC library build for CPU Rev 2.0.