Other Parts Discussed in Thread: TMS320C5535, , CC3200, BOOST5545ULP, MSP430FR5994
Hi All,
First post from a complete and absolute noob here wanting to build an Active Noise Cancellation Algorithm using a TMS320C5535 DSP. So I was planning to use the TMDX5535EZDSP development board (budget reazons), but then I realised that it might not be suitable for my problem, so I'll want get some of your feedback.
The basic problem is:
1. Input 1: Incoming sound (Microphone 1)
2. Output: Generate an inverted wave of #1 ( Speaker/Actuator )
3. Input 2: Read remaining sound after the actuator, which is used to adaptively adjust the gain of 1 (Microphone 2).
So the second reading (#3) is totally necessary to make the circuit work/test. However this board only has one Mic-Input. So, my idea is/was that stereo sound is irrelevant for my application, just need one channel, so say that I could use the left-channel for Input-1 and the right-channel for Input-2.
Question: Does that sound feasible at all? If not, which "budget and Active" development board would you recommend instead for my application?
Thanks!