Hi TI Experts.
Please let me confirm the following questions of relating to I2S usage on C5517.
[Question.1]
Is there any influence for the device operation by disabled the I2S function by ENABLE bit on I2SxSCTRL and setting the I2S registers like I2S0SRATE, I2S0SCTRL?
[Background]
My customer are thinking that will disable the I2S function by ENABLE bit on I2SxSCTRL register after finish to use this. So, they think that some registers values of I2S will remain after disabled the I2S function. So, they would like to know whether there is any problem by remaining those values on I2S registers.
[Question.2]
Is there any problem to set the I2SnSRATE value even though the I2S function on C5517 was set Slave? Or should customer set 0x00 values for this register in this case(Use case is slave) ?
If you have any questions, please let me know.
Best regards.
Kaka