Hi,
I have a question about VC5506 and C5517.
Our customer are using VC5506 on their system.
But they are planning to replace from VC5506 to C5517 and they have question about C5517 I/O voltage.
They want to supply 3.0V to C5517 DVDD(I/O voltage)
In their system, other external devices need 3.0V.
So,they are also supplying 3.0V for VC5506 I/O voltage(DVDD).
3.0V is in the range of VC5506 DVDD(Device supply voltage), so there are no problem.
VC5506 DVDD range is 2.7V - 3.6V.
If they replace to C5517, can they still use 3.0V for C5517 I/O voltage?
From datasheet of C5517, I/O voltage is 1.8V/2.75V/3.3V.
But 3.0V is in the range of each 2.75V and 3.3V.
2.75V range is "2.48V - 3.02V".
3.3V range is "2.97V - 3.63V.
best regards,
g.f.