Hi,
I have performed few tests on TIesr keeping in mind few cases based on different scenarios. The report table for simple words is below.
Each test word is tested using custom trained engine. Even if TI trained engine is used similar results are observed.
Each scenario includes 5 repeated tests . Scenarios include below things:
- Using only the test word every time.
- Using single words other than test word. Here points are given if the word is not detected.
- Using test word in a sentence.
- Using sentence without the test word.
Test Scenario - Total 5 each | ||||||
Test No | Word Type | Word | Only 1 word (High is good) | Other words (High is good) | Word in a sentence (High is good) | Other words in sentence (High is good) |
1 | Simple | yes | 3 | 4 | 3 | 3 |
2 | no | 5 | 1 | 1 | 3 | |
3 | okay | 3 | 2 | 2 | 2 | |
4 | lock | 5 | 4 | 2 | 1 |
Any suggestions on improving this?
Regards,