Part Number: TMDXEVM5515
Hello,
according to the modes below, can it be configured by our own? For example, in Parallel Mode 5, can I change it from 'LCD 8 bit + SPI (CS0) +UART ' to 'GPIO 12 ~17 + + SPI (CS0) +UART '
typedef enum {
SERIAL_PORT_MODE0 = 0, // MMC/SD
SERIAL_PORT_MODE1 = 1, // I2S0/1 + GPIO4/10, 5/11
SERIAL_PORT_MODE2 = 2 // GPIO 0 ~ 5/ 6 ~11
} SerialPortMode;
typedef enum {
PARALLEL_PORT_MODE0 = 0, // LCD 16 bit
PARALLEL_PORT_MODE1 = 1, // SPI (CS0,1,2,3) + GPIO 12 ~17 + I2S2 + UART
PARALLEL_PORT_MODE2 = 2, // LCD 8 bit + GPIO 18 ~31
PARALLEL_PORT_MODE3 = 3, // LCD 8 bit + SPI (CS0) + I2S3
PARALLEL_PORT_MODE4 = 4, // LCD 8 bit + I2S2 +UART
PARALLEL_PORT_MODE5 = 5, // LCD 8 bit + SPI (CS0) +UART
PARALLEL_PORT_MODE6 = 6 // SPI (CS0,1,2,3) + GPIO 12 ~ 17 + I2S3
} ParallelPortMode;