Hi, all,
We evaluate TMS320C5517 DSP.
We are using the DSPs generating external clock and disabled RTC.
We try the DSP will wake-up from IDLE3 state with INT0 pulse.
When SYSCLK=0 in PCGCR1, the DSP doesn't accept INT0.
However, when SYSCLK=0 and EMIFCG=0, the DSP accept INT0 and CPU wake-up from IDLE3.
I'd like to know why EMIF module is concern to the wake-up process.
And is it okay to use this wake-up process without RTC?
Regards,
Massa