Other Parts Discussed in Thread: CODECOMPOSER
Tool/software: Code Composer Studio
Hello, my name is Alexander. I have a problem with setting up interrupt vectors for external interrupts My CodeComposer Studio version is 5.5.0. I use a SPRA036 document to do it. When i build the project i get the error:
<Linking>
undefined first referenced
symbol in file
--------- ----------------
_c_int2 ./vecs.obj
_c_int3 ./vecs.obj
_c_int4 ./vecs.obj
_c_int5 ./vecs.obj
error #10234-D: unresolved symbols remain
>> Compilation failure
error #10010: errors encountered during linking; "VC5416.out" not built
gmake: *** [VC5416.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Can someone send me the correct versions of the files, which i attached here? Or can you give me an example?drive-download-20171020T114727Z-001.zip Thank you.