Hi TI Experts,
Please let me confirm the following question.
Note: This question is related to the following E2E post.
[Question.1]
Would you please teach me the timing or condition to happen the interrupt of INTRTX?
I think that this will happen when device complete transmitting the FIFO data to Host.
[Question.2]
If my understanding is correct, what do you think the cause to happen the INTRX(EP1TX) interrupt twice within very short duration(40us) even though the data did not complete transmitting when the CPU clock was 200MHz?
At this time, the CPU over-write the data on FIFO even though the data did not complete transmitting. If you need more data to resolve this issue, please let me know. They have used the following environments.
Board: Custom board
CAF version: v02.00.02.04
CSL version: v3.07.00
[Question.3]
Could you please reproduce this issue by modifying the CAF in order to run the C5517EVM on your side?
We must answer this question by next Tuesday in Japan time. So, please help us.
Best regards.
Kaka