We made an expansion card for the VC5505 USB Stick with a sd Card interface. Using CCS 4.1.2.0027 we tried the SD card examples in the library. The programs csl_mmcsd_intr_example, csl_mmcsd_SDCardExample (polled) and csl_mmcsd_dma_example are build without problems but do not work. The intr and the dma example have an error when executing the function MMC_setBlockLength, status = 0xfff6. The polled example has an error when executing SD_setBusWidth, also with status 0xfff6.Has anyone successful tried the sd card examples for a VC5505 USB Stick?
The example with the file system was not possible to build because a ATA driver library is missing and there is no project to create the library. Is there elsewhere a project for the library?
Thanks in advance