Part Number: TMS320C5545
Tool/software: Code Composer Studio
Greetings Good People of E2E forum!
I am Akshay. I am using TI's latest DSP board, C5545 board. I am planning on using it with MSP432P401R board. I would want to develop DSP applied Embedded system applications for my Laboratory. For this initially, I would want to perform a DTMF signal detection experiment on the C5545. I need to access the input and output ports of the C5545 board to get this done. I also would want to use the bluetooth module but not for the equalizer app. I would want to share a picture using an Apple phone. So how does this work then? Can somebody guide me how I could do this/ I have previously worked on C6713 DSK and it was simple there. I have the code for the C6713DSK is there something similar to that for this board? If there is I would be happy. The platform I am working on is:
Windows OS: Windows 7
CCS version: CCS v6.2.0
CSL files: CSL 3.08
Code For C6713 DSK:
#include "DSK6713_AIC23.h" // codec support
Uint32 fs=DSK6713_AIC23_FREQ_8KHZ; //set sampling rate
#define DSK6713_AIC23_INPUT_MIC 0x0015
#define DSK6713_AIC23_INPUT_LINE 0x0011
Uint16 inputsource=DSK6713_AIC23_INPUT_LINE; // select line in
Also, when I try to generate to follow the guidelines in the Softwares user's manual top generate the C55 DEMO file I get this error which says TIesrEngineC55 has not been executed. And the error shows mem.h has not been found.; Can somebody help me with these two problems. I would be more than happy if somebody is up for a SKYPE or web-ex session to help me with this. I available 24/7 at your convinenience. Please let me know.
Thank you
Akshay.