Hello all,
I bought TMDXMDKPO8328 Pulse oximetry analog front-end module and 5515EVM,when i load the spo2.out from MDK_SpO2System_C55515EVM i got 45 errors and 19 warnings.Once i load the .out file into 5515EVM and run it ,but the pulse wave and spo2&pulse rate display were wrong,the details are as follows:
1.the application display
2.LCD display
I am not sure wether i have load the code to the 5515EVM or not,and the results is wrong.Someone who can tell me what is the matter of it and what is the correct way to import a project and run it as its right way.I am a beginner of 5515 and does not very familiar with CCSV4,another thing is wether the BootImageCreation.zip is necessary if i want to run the program.Thank you for your details!
Regards,