I am using the TMS320CC5515 EVM connected to the front-end Spo2_FE_Rev_2 and I have the project for that on my PC, I download the .out (either the file that came with the project or one that I build from the files. I'm using CCS v3.3 and it appears to load correctly. When I run the program it seems to be stuck in the vectors.asm on
wait_pll:
AC0 = *port(PLL_CNTL3)
AC0 = AC0 & 0x0008
if(AC0 == 0) goto wait_pll
What am I doing wrong? The first time I ran it out-of-the-box, with no debug connections the OLED worked.
Rob Reasons