• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Digital Signal Processors (DSP) » C5000 Ultra Low Power DSP » C5000 Ultra Low Power DSP Forum » All Tags » gpio
Share
C5000 Ultra Low Power DSP
  • Forum
  • Announcements

Browse by Tags

C5000 Ultra Low Power DSP

Welcome to the C5000 Ultra Low Power DSP Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
gpio
  • 5505 ezDSP
  • 5515
  • ADC
  • aic3204
  • C5504
  • C5505
  • C5505 eZdsp
  • C5509A
  • C5515
  • C5535
  • C55X
  • C55XX
  • CCSv4
  • CSL
  • DMA
  • DSP
  • eZdsp
  • I2C
  • I2S
  • Interrupt
  • McBSP
  • sample code
  • SPI
  • TMS320C5515
  • TMS320VC5505
Related Posts
  • Forum Post: Re: C5509A GPIO_pinWriteAll()

    TommyG TommyG
    Audi, According to the CSL Product Folder ( http://focus.ti.com/docs/toolsw/folders/print/sprc133.html ), the latest version of the CSL for the C5509A device is v2.31.00.9 which was released on March 24, 2005. The latest Reference Guide (SPRU433J) is indeed dated September 2004. I see in Table...
    on Aug 2, 2010
  • Forum Post: TMS320VC5401 HP1(GPIO),Uart Registers addressing Details

    Ashwin Panchal Ashwin Panchal
    Hi, After working on TMS320VC5505 now i am working on TMS320VC5401. But during this development i am facing some problems, Generally in 5505 to access the peripheral registers (like GPIO, I2S, UART and Timers etc etc) we need to declare it's address with their name like below register decleration...
    on Nov 25, 2010
  • Forum Post: C5515 GPIO input timing

    Bernhard Funck Bernhard Funck
    We want to connect an ADC to the GPIO of the C5515 and we want to achieve a sample rate as high as possible. According to Table 6.54 of the data sheet the minimum pulse width is one or two cycles depending on wether the input is activ or inactive. That means that the minimum possible sampling rate is...
    on Nov 1, 2010
  • Forum Post: Why can't use second McBSP- McBSP1 as GPIO in C5510 DSK

    Shanjie Chen Shanjie Chen
    I can configure the McBSP0 as GPIO and read status in C5510 DSK using following codes: (I add the code in the example program: CCStudio_v3.1\examples\dsk5510\bsl\led, led project) hMcbsp0 = MCBSP_open(MCBSP_PORT0,MCBSP_OPEN_RESET); MCBSP_RSETH(hMcbsp0,SPCR1,0x0000); MCBSP_RSETH(hMcbsp0,SPCR2,0x0000...
    on Nov 29, 2010
  • Forum Post: I need these pins for the ezDSP TMS320VC5505

    Timothy Sapio Timothy Sapio
    http://imgur.com/RXQQQ They are referred to in the documentation as "test pins". They are not the standard pin size that everyone else in the world uses, and there are no part numbers mentioned in the documentation. How do I turn these holes for pins into pins???
    on Jul 9, 2011
  • Forum Post: Persistant errors EVERY TIME I try to build a project from examples.

    Timothy Sapio Timothy Sapio
    **** Build of configuration Debug for project CSL_GPIO_OutputPinExample **** C:\TI\ccsv4\utils\gmake\gmake -k all 'Building target: CSL_GPIO_OutputPinExample.out' 'Invoking: Linker' "C:/TI/ccsv4/tools/compiler/C5500 Code Generation Tools 4.3.9/bin/cl55" -v5505 -g --define="_DEBUG"...
    on Aug 10, 2011
  • Forum Post: Interrupt Driven Program does not work at full speed.

    Timothy Sapio Timothy Sapio
    TMS320C5505 ezDSP Rev.D I am using the I2S bus in DMA mode and am trying to merge in code that sends signals to GPIO pins. When I step through the program in the debugger, everything works fine, but when I play the program at full speed, the DMA interrupt flags are cleared by the time the program...
    on Dec 31, 2011
  • Forum Post: How to use 5502 pgpio port?

    bob jiang bob jiang
    Hello,everyone: I am using tms320vc5502. In datasheet that is described :The XBSR configures the Parallel Port Mux and the Host Port Mux at reset based on the state of theGPIO6 pin at reset. When GPIO6 is high at reset, the Parallel Port Mux will be configured to support the 32-bit EMIF and the Host...
    on Feb 17, 2012
  • Forum Post: RE: C5504 pin multiplexing issues

    Theodore Wolff Theodore Wolff
    Thanks for the questions, John. My answers to each are: Good point about being clear regarding Mode 0 in the EBSR:PPMODE table. We will add this column to the C5515/14/05/04 datasheets in our next update. Your assumption is correct. We will also add GPIO[17:12] to the description of the EBSR Register...
    on Aug 10, 2012
  • Forum Post: Problem with UART

    Florian Parkitny Florian Parkitny
    Hello, i use the TMS320C5535 eZdsp USB evaluation board and have some problems with the UART. I need the GPIO Pins (actually two Led's) for time measurement. Anymore i want to use the UART to send results (computed results with the FFT-Function) to the Hyperterminal. One of the functions run...
    on Aug 22, 2012
  • Forum Post: Call flag to oscillograph by GPIO pin TMS320C5515

    Dmitriy Luk'yanov Dmitriy Luk'yanov
    Hello, I have TMS320C5515 eZDSP USB Stick and I testing my coder with it. So this is part of my code: usbstk5515_gpio.h ... %This line start transfer signal on pin Encoder(inS, difS); Decoder(difS, outS); %This line stop transfer signal on pin ... Which function does this? USBSTK5515_GPIO_setDirection...
    on Jan 10, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use