• Jul 7, 2017

    Processor SDK 4.0 Released (AM57x, AM437x, AM335x, K2x, C66x, C674x, OMAP-L13x)

    Processor SDK 4.0 is now available for download! For migration information, see RTOS migration page or Linux migration page . The Processor SDK (Software Development Kit) is a unified software platform for TI embedded processors providing easy setup a...
    • Apr 6, 2017

    Processor SDK 3.3 Released (AM57x, AM437x, AM335x, K2x, C66x, OMAP-L13x)

    Processor SDK 3.3 is now available for download! For migration information, see RTOS migration page or Linux migration page . The Processor SDK (Software Development Kit) is a unified software platform for TI embedded processors providing easy setup a...
    • Oct 8, 2016

    Processor SDK 3.1 Released (AM57x, AM437x, AM335x, K2x, C66x)

    Processor SDK 3.1 is now available for download! For migration information, see RTOS migration page or Linux migration page . The Processor SDK (Software Development Kit) is a unified software platform for TI embedded processors providing easy setup a...
    • Jul 14, 2016

    Processor SDK 3.0 Released (AM57x, AM437x, AM335x, K2x, C66x)

    Processor SDK 3.0 is now available for download! For migration information, see RTOS migration page or Linux migration page ., and for a full list of supported devices, see Processor_SDK_Supported_Platforms_and_Versions The Processor SDK (Software Dev...
    • Jan 18, 2016

    Processor SDK 2.0.1 Released (AM57x, AM437x, AM335x, K2x, C66x)

    Processor SDK 2.0.1 is now available for download! This release primarily adds support for devices from the KeyStone architecture: C665x, C667x, K2E, K2H, K2K, and K2L. For migration information, see RTOS migration page or Linux migration page . The P...
    • Oct 1, 2015

    MCSDK 3.1.4: Maintenance Update for KeyStone II devices (K2H, K2K, K2E, K2L)

    MCSDK 3.1.4 is now available for download ; this is a maintenance update for the R3.1.0 release stream. The major updates from the last release are: High Performance Compute support, including ARM/Linux OpenCL and DSP/RTOS OpenMP runtime packages Cer...
    • Apr 28, 2015

    Keystone II Bootloader Examples

    Keystone II bootloader examples are now availalbe for download. Source code published to external git: https://git.ti.com/keystone2_boot_examples Documentation: http://processors.wiki.ti.com/index.php/KeystoneII_Boot_Examples Software Features ...
    • Mar 30, 2015

    MCSDK 3.1.3: Maintenance Update for KeyStone II devices (K2H, K2K, K2E, K2L)

    MCSDK 3.1.3 is now available for download ; this is a maintenance update for the R3.1.0 release stream. The major updates from the last release are: IPC MessageQ transport for device-to-device (SRIO) and efficient intra-device Linux (Navigator) Y.173...
    • Oct 5, 2014

    MCSDK 3.1.1: Maintenance Update for KeyStone II devices (K2H, K2K, K2E, K2L)

    MCSDK 3.1.1 is now available for download ; this is a maintenance update for the production R3.1.0 release. The major updates from the last release are: TransportNetLib: Port mirroring and capture, see PA LLD release notes for details TransportNetLib: QoS dual shaper, see PA LLD release notes for details AETLib: An AET interrupt is generated upon detecting a CPU pipeline stall Bug fixes (see Release...
    • Aug 8, 2014

    MCSDK 3.1 Production Release Available for Additional KeyStone II Devices

    MCSDK 3.1.0 is now available for download . This is the production release of the R3.1 stream adding support for K2L and K2E. This release builds on top of MCSDK 3.0.4, see Migration Guide for information on migrating from that release for K2H/K2K users. See Release Notes for more information. This release provides foundational software for all currently available KeyStone II devices and EVMs: Platform...
    • Apr 25, 2014

    MCSDK 3.0.4: Maintenance Update for K2H/K2K

    MCSDK 3.0.4 is now available for download ; this is a maintenance update for the production R3.0.0 release. The major updates from the last maintenance release, MCSDK 3.0.3, are: Update to Yocto 1.4 MPM Transport enhancements for HyperLink, EDMA3 EDMA3 user mode LLD, MMAP/MPAX user mode LLD Trace framework enhancements: Local contract creation in ARM UIO Module driver to support uio based user space...
    • Nov 25, 2013

    MCSDK 3.0.3: Maintenance Update for K2H/K2K

    MCSDK 3.0.3 is now available for download ; this is a maintenance update for the production R3.0.0 release. The major updates from the last maintenance release, MCSDK 3.0.2, are: Linux kernel update to LTS 3.10 HyperLink user mode LLD and MPM-Transport MMAP/MPAX DSP LLD Support for EVMK2H Bug fixes (see the Release Notes for full list) The major updates in past maintenance release from the production...
    • Oct 3, 2013

    MCSDK 3.0.2: Maintenance Update for K2H/K2K

    MCSDK 3.0.2 is now available for download ; this is a maintenance update for the production R3.0.0 release. The major updates from the last maintenance release, MCSDK 3.0.1, are: Linux Kernel 10G Interface Uboot 512 MB NAND Shared library for PA/SA/Transport net lib user space components Update to latest CCS 5.5 Bug fixes (see the Release Notes for full list) The major updates in past maintenance...
    • Sep 4, 2013

    Vision Library (VLIB) v3.0.0.7 Release with optimized C66x Functions

    We are pleased to announce this release of the Vision Library (VLIB) for C64x+/C674x/C66x processors. This is the first release to offer optimized C66x DSP kernels. The library is available royalty-free and is downloadable here: http://software-dl.ti.com/libs/vlib/latest/index_FDS.html VLIB is a software library of more than 40 kernels from Texas Instruments that accelerates video analytics development and increases...
    • Aug 1, 2013

    MCSDK 3.0.1: Maintenance Update for K2H/K2K

    MCSDK 3.0.1 is now available for download ; this is a maintenance update for the production R3.0.0 release. The major updates from the production release, MCSDK 3.0.0, are: User space PA/SA LLD multiprocess support Transport net lib enhancements for inflow IPSEC offload and sideband crypto offload support in kernel Ethernet time stamping (CPTS) support for PTP User space contiguous memory allocator ...
    • May 31, 2013

    MCSDK 3.0 Production Release Available for KeyStone II Devices

    MCSDK 3.0 production release is now available for download . This release provides foundational software for K2H and K2K KeyStone II devices. It encapsulates a collection of software elements and tools intended to enable customer application development. The foundational components include: SYS/BIOS real-time embedded operating system on DSP cores Linux high-level operating system running on ARM A15 cluster...
    • Apr 30, 2013

    MCSDK 3.0 Beta Release Available for KeyStone II Devices

    MCSDK 3.0 Beta is available for download . The MCSDK provides foundational software for TI KeyStone II device platforms. It encapsulates a collection of software elements and tools intended to enable customer application development and migration. The foundational components include: SYS/BIOS real-time embedded operating system on DSP cores Linux high-level operating system running on ARM A15 cluster (SMP...
    • Mar 4, 2013

    Release of Desktop Linux SDK v1.0

    This is the Production release for R1.0.0 Desktop Linux SDK The Desktop Linux SDK package provides a software development environment to help offload highly compute intensive processing from a desktop Linux PC to power efficient TI C66x multi-core DSPs through the PCIE interface. For more information, see http://software-dl.ti.com/sdoemb/sdoemb_public_sw/desktop_linux_sdk/latest/index_FDS.html
    • Mar 4, 2013

    Release of MCSDK Video v2.1

    This is a production release for the R2.1.0 Multicore Video Infrastructure Demo Built on MCSDK. This package of Multicore Video Infrastructure Demo Built on MCSDK (called as MCSDK Video in short thereafter) provides software development environment to implement and demonstrate real-time video applications on TI C66x multi-core DSPs. The MCSDK Video 2.1 is built leveraging two SDKs. BIOS-MCSDK [SDK is DSP internal...
    • Nov 13, 2012

    TI provides self-paced online training that introduces the primary components of the KeyStone II family of SoC devices

    TI provides self-paced online training that introduces the primary components of the KeyStone II family of SoC devices . KeyStone II SoC Overview provides a high-level view of the device architecture, including the C66x and ARM Cortex-A15 processors, memory and transport topologies, networking and interface enhancements, as well as power saving and debug features for the KeyStone II family of C66x multicore devices...
    • Nov 13, 2012

    BIOS-MCSDK 2.1.2: Maintenance update for C66x BIOS-MCSDK

    BIOS MCSDK 2.1.2 is available for download ; this is a maintenance update for the production R2.1.0 release. This update can be manually downloaded or automatically downloaded directly from CCS using Eclipse Update Manager; see the BIOS MCSDK User's Guide for details on setting up automatic software updates . The major updates from the last maintenance release, BIOS MCSDK 2.1.1, are: Introduction of OpenEM...
    • Oct 6, 2012

    BIOS-MCSDK 2.1.1: Maintenance update for C66x BIOS-MCSDK

    BIOS MCSDK 2.1.1 is available for download ; this is a maintenance update for the production R2.1.0 release. This update can be manually downloaded or automatically downloaded directly from CCS using Eclipse Update Manager; see the BIOS MCSDK User's Guide for details on setting up automatic software updates . The major updates from the production release, BIOS MCSDK 2.1.0, are: Production quality software...
    • Sep 6, 2012

    BIOS-MCSDK 2.1.0: OpenMP for C66x Multicore DSP

    The production release of BIOS-MCSDK 2.1 is available for download . This release introduces OpenMP as a multicore programming methodology for TMS320C6678 and TMS320C6670 . This release can be manually downloaded or automatically downloaded directly from CCS using Eclipse Update Manager; see the BIOS-MCSDK User's Guide for details on setting up automatic software updates . The BIOS Multicore Software Development...
    • Jul 19, 2012

    Integre Technologies Announces HyperLink DSP Interface FPGA Core

    Integre Technologies ( http:/ www. integre tek.com/ ) has announced the release of the IP-HyperLink high speed digital signal processor (DSP) interface core for both Altera and Xilinx device families. The announcement can be found here http://www.prweb.com/releases/2012/6/prweb9643885.htm Details regarding the HyperLink DSP Interface from Integre Technologies can be found here http://www.integretek.com/products...
    • Jun 30, 2012

    BIOS-MCSDK 2.1.0 Beta Available for C66x DSP OpenMP Support

    BIOS MCSDK 2.1.0 Beta is available for download . This release introduces OpenMP support for TMS320C6678 . Note that this is a beta quality release; for the production quality release of C66X, see BIOS-MCSDK 2.0.9 . The major updates from the baseline release, BIOS MCSDK 2.0.9, are: OpenMP runtime component CGT 7.4 Beta2 OpenMP version of Image Processing Demo The BIOS Multicore Software Development...