This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

the connection between C6474 and Virtex using SGMII without PHY

In TMS320C6474, I would like to connect directly between C6474 and Virtex6 using  MAC of SGMII without PHY.

It based on the following documentation on page 29.

http://focus.ti.com/lit/an/spraaw7a/spraaw7a.pdf

It describe to connect C6474(Master) and C6474(Slave) using SGMII.

Does it connect betweek Virtex& and C6474 using SGMII without PHY?

If possible, is there any sample program for that?