Dear people of the forum, I was working on a program that uses 3 cores of a c6472. This sample program works ok from the CCSv4 and the emulator. It does not work (BOOT) from the NAND flash memory that brings the EVM. If we change the sample program to use only the core 0, the sample works from the CCSv4 and from the NAND memory (DIPSWITCH Boot selection).
Then I thought it was a good idea to put at the disposal of all the example program. In this way the contributions of all we could to run this program (attached below) with the 3 cores from the NAND memory and this serves as an example to people (like me) who do not have enough knowledge to do so.
Regrads
ENG. Electronics
Ricardo