Hi all,
Is there a way to sync the external mem (DDR) between the 3 C6474 cores under CCS3.3 simulator?
Thanks,
Haim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Haim,
Can you detail the meaning of 'Sync'?
REgards,
Nizam
Hi Nizam,
The DDR2 should be R/W from the same address by the 3 cores (0x80000000) but what happen is that if I'm writing to the DDR at address x by core 0 I'm getting different data at address x from core 1 or 2 where it should be the same data,
Please let me know if additional info is needed,
Many Thanks,
Haim
Hi Haim,
You seem to notice data incoherencey across different cores, for the same memory location of DDR2.
This may happen because of the caches in the system. You might notice that a given address 'x' is cached in each Core's (memory-system's) L1/L2 cache. In such a state, updates to the address 'x' by a given core is updated locally to the cache'ed value, than the DDR value. Unless the cache contents are fluxhed to DDR2 memory, other core may read a stale data to address 'x'.
Hope this helps. LMK if you need more details on flushing the cache and so on.
Regards,
Nizam
Nizam,
That is a good thought, but Haim mentioned he was using the simulator and not an actual target. The issue here is that you have three simulated cores running in three different instances of CCS via Parallel Debug Manager. Is there anyway to sync up the contents of "DDR" located at 0x80000000 between each of these three cores in the simulator? I am assuming this is not doable, but hoping for expert feedback [:)]
Hi Nizam,
You are correct without using the L2 cache the issue is solved (I didn't checked this yet with the simulator) but as I want to use the cache can you please let me know where I can find more info regarding the cache handling,
Many Thanks,
Haim
I am glad I was wrong here!
Regarding cache handling there are several articles on the Embedded Processors Wiki that may help including:
- Cache Management
- Enabling Cache on C64x+
But you may also want to view the document on the cache for your specific device as this sometimes contains device-specific information as well.