Hi,
I have some problems and I need help please.
these days , I found therr are new Application Notes on TMS320C6474:
I found there are 2 new Lib for us,Direct I/O Library and Using the TMS320C6474 Antenna Interface (AIF) for Inter-DSP Communication
On the https://gforge.ti.com, I found the two project I want:
1. "AIF Example Code for C6474" on https://gforge.ti.com/gf/project/aifinterdsp/
2. "6474 SRIO DirectIO Library"
I really need them,and I want to download them.
But the project "6474 SRIO DirectIO Library" can't be opend,
and the project "AIF Example Code for C6474"can't be check out
(it means when I check out using the TortoiseSVN,it's turn out to be an error
says:
"Error: PROPFIND request failed on '/svn/c6474aif'
Error: PROPFIND of '/svn/c6474aif': 301 Moved Permanently (http://gforge.ti.com) ")
And I found there is no body who did the check out.
I really want these Library,please help me
Is there any kindhearted can help me please?
Think you very much!