Hi,
using CCSv5.2 I build my project for:
Family: C6000
Variant: C6-Integra - C6A8168
I get no errors for this. Build Successful.
But when I build it for:
Family: ARM
I get several Assembler errors as:
"C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 10544: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |841| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 10550: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |842| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 10557: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |843| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 10565: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |844| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11053: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |889| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11059: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |890| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11422: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25616] ; |930| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11431: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25616] ; |934| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11435: [E0200] Offset out of range, must be [-4095,4095] LDR A2, [V4, #25636] ; |936| "C:\DOCUME~1\nly37782\LOCALS~1\Temp\0432010", ERROR! at line 11455: [E0200] Offset out of range, must be [-4095,4095] LDR V9, [V4, #25632] ; |938|
Any thoughts on how to resolve these errors?
Hello,
I believe you may have posted in the wrong forum. Can you please confirm you are using a Hercules MCU device?
Regards,
Karl
Given the time since the last post to this thread, it is assumed that the post was posted to the wrong forum as suggested and the thread will be closed.
Thanks and Regards,
Chuck Davenport
If this response answers your question, please indicate it by verifying the suggested answer when provided.