I have downloaded the project from http://processors.wiki.ti.com/images/0/05/NDK2_2_dual_evm6474.zip,then built it under CCS4.2 with necessary .h file .The program produce following message:
--------------------------------------------------------------------------------------------
TCP/IP Stack 'Hello World!' Application
emac_init: core 0, port 0, total number of channels/MAC addresses: 1/1
MAC addresses configured for channel 0:
3C-2D-B7-23-14-75
SGMII reset successful................................
SGMII config successful...........................
emac_open core 0 port 0 successfully
Registration of the EMAC Successful, waiting for link up........
Network Added: IF-1:10.11.169.11
Port 0 Link Status: 1000Mb/s Full Duplex on PHY 1
--------------------------------------------------------------------------------------------
How to test the project is working properly? I am 'ping' from the PC is not successfully.
when I click the halt button to see which step the code is running at, it always appears the following picture.
Is this correct?
How to solve the problem.thanks