Hi,
I run the helloworld from the mcsdk on the smt372t with carried board smt111. The console print message as follows:
TCP/IP Stack "Hello World!" Application
Registration of the EMAC Successful, waiting for link up ....
Network Added: If-1:192.168.1.11
port 0 link status: 1000Mb/s Full Duplex on PHY 1.
But when I send messages from PC to DSP core0, it does not receive any packages.
Ping from the PC to DSP, it has no response.
What is the problem with the project.Could you please help me . Thanks .