Hello everyone,
I am trying to install and use MCSDK on a Linux system (bios_mcsdk_bios_mcsdk_02_01_02_06). Most of the installation goes right for different versions of CCS. Nevertheless, when I try to Add Discovered Products I get something like:
Operation details
Cannot complete the install because some dependencies are not satisfiable
com.ti.biosmcsdk.feature.group [2.1.2.6] cannot be installed in this environment because its filter is not applicable.
As I mentioned, I had tried with different CCS version: 5.4, 5.5, 6.0 and 6.1, with the same result.
So my question is: which is the right CCS I should use to properly have the MCSDK for developing multicore applications?
Thanks in advance for all the informations and hints you can provide me.