hi,
I tested the SRIO example "srio_evm_dio_example" in the common CCS project without RTSC, it worked, but when I migrate the example to the CCS project with RTSC, the example of SRIO write function doesn't work, that means my FPGA program cann't received the data from DSP.
In my CCS5.4 project with RTSC, I didn't start BIOS service, the example code just like the project without RTSC, means that the only difference is the CCS project whether used RTSC.
I'm confused with this problem, will someone can give me some advice?
The "srio_evm_dio_example" is as same as the question in the follow website.
Thanks.