Hi All,
I have trouble finding information what value the srcTID/targetTID fields will be set for SRIO packets sent by the DSP.
I have checked the following documents so far: "TMS320C6472/TMS320TCI648x DSP Serial RapidIO (SRIO) User's Guide" and "TMS320C6472 Chip Support Library API Reference Guide"
Page 37 of the SRIO user gide states: “Some fields, such as the RapidIO srcTID/targetTID field, are assigned by hardware and do not have a corresponding command register field”, which implies this might be a random number assigned by hardware.
I can also only assume that targetTID will take the value of the corresponding request packet’s source transaction ID, but haven't found any confirmation on that either.
I'm happy to dig further if pointed to the right direction, but a direct answer is also more than welcome. Thanks in advance,
Marton