Recently we started porting a project for a C6474 from DSP/BIOS (CCS3.3) to SYSBIOS (CCS6). One of the used libraries is EDMA LLD. In the original project we used version "edma3_lld_01_11_02_05". Now the latest version is edma3_lld_02_11_05_02, but support for the C6474 seems to have been removed! The latest version on the git.ti.com repo also does not show the C6474.
Could someone comment on this and suggest a solution? I posted a LLD related question at the time which caused me to believe the C6474 would be supported.
Thanks,
Dirk