we are working on some project and now we have installed all the software on a second computer. However this doesn't works as expected. I can compile the software and i can step through using the simulator however if i press continue i get evrythime an exeption is stated below.
Can someone help me to explain? By the way on the other, previous computer I don't get this exception.
[C66xx_0] e=176
A0=0xfffffee0 A1=0x0
A2=0x1 A3=0x9f8f1070
A4=0x9f8f1070 A5=0x9f8f1da0
A6=0x9f8f08a4 A7=0x0
A8=0x0 A9=0x3
A10=0x8 A11=0x0
A12=0x0 A13=0x0
A14=0x0 A15=0x0
A16=0x9f8f1190 A17=0x0
A18=0x9ee880e0 A19=0x80000
A20=0x6c A21=0x4c
A22=0x0 A23=0x0
A24=0x0 A25=0[C66xx_0] x0
A26=0x0 A27=0x0
A28=0x0 A29=0x0
A30=0x4 A31=0x1e3b
B0=0x0 B1=0x0
B2=0x800 B3=0x9f823a8c
B4=0x9f8f1db0 B5=0x9f8f024c
B6=0x10 B7=0x0
B8=0x9f8e0d80 B9=0x3a
B10=0x0 B11=0x0
B12=0x0 B13=0x0
B14=0x9f8fc600 B15=0xffffffe0
B16=0x30 B17=0x9f8e100c
B18=0x3 B19=0x[C66xx_0] 0
B20=0x69 B21=0x2e2
B22=0x2e20000 B23=0x0
B24=0x0 B25=0x3000
B26=0x3000 B27=0x0
B28=0x0 B29=0x0
B30=0xff B31=0x90
NTSR=0x1000f
ITSR=0x0
IRP=0x0
SSR=0x0
AMR=0x0
RILC=0x0
ILC=0x0
Exception at 0x9f8f1078
EFR=0x2 NRP=0x9f8f1078
Internal exception: IERR=0x8
Op[C66xx_0] code exception
ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x9f8f1078, sp = 0xffffffe0.
To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enab[C66xx_0] lePrint = true;'
xdc.runtime.Error.raise: terminating execution