i am student and working on condition monitoring project.
i need a solution like TI launch pad which can be easily programmable. But it should be capable of sensing analog voltage(analog input) at the rate of around 100 MS/s(100 Million Samples per second). Also it should be able to produce analog voltage(analog output) at the rate of 100 MS/s.
There is no restriction on processor type. it doesn't matter if it is Microcontroller or DSP or anything else.