Hi,Expert
We are currently implementing sRIO communication at ARM (SYS / BIOS), but are there sRIO drivers for ARM (SYS / BIOS)?
I am implementing it using the API (* 1) of the sRIO driver in pdk, but since there is no library for ARM (SYS / BIOS), it is a build error in CCS .
After checking the error contents, it seems that the ti.drv.srio.aa15fg file is required as library, but it can not be found even if it searches in pdk.
(The attached file becomes error information of CCS.)
I am using the API in the following folders.
\ti\pdk_k2hk_4_0_6\packages\ti\drv\srio
It also did not exist in the latest PDK below.
\ti\pdk_k2hk_4_0_8\packages\ti\drv\srio\lib
Best Regards,
Honma