I am not able to understand the differences in handling interupts.
An ISR can be hooked in 3 ways [CSL_intcPlugEventHandler, CpIntc_dispatchPlug and CSL_intcHookIsr], what is purpose and when [at what stage]. Can Some Member from Ti/Public Kindly writeback a Detailed reply on this.
please reply to below points
1. differences among them.
2. when to use what.
3. Any guidelines for point 2.
4. ease of use.
5. Any major configs/settings to be taken care.
Thanks
RC Reddy
RC,
Which device are you using? Which software versions are you using?
Following the examples that are provided with the software packages will show you how to use these functions.
Regards,RandyP
Search for answers, Ask a question, click Verify when complete, Help others, Learn more.
Hi Ran,
I am using c6670.
CCSV5 [latest 69 version], MCSDK - 02_00_09_21.
1. In Hyperlink, CSL_intcPlugEventHandler is used for hooking ISR.
2. In SRIO, for handling ISR, CpIntc_dispatchPlug is used.
3. In AIF2, CSL_intcHookIsr is used for hooking ISR.
all above three functions based example projects are from Ti in PDK folders under c6670.
I couldn't understand the situation/context in which each of the above functions is used. Kindly answer below questions
My main question stands the same.
2. when to use which ISR HOOKING FUNCTION.
4. Ease of use.
CSL_intcHookIsr mapping ISR function to hardware interrupt vector, the function should be defined as "interrupt".
CSL system maintatins its self ISR-vector mapping table as below,
_CSL_intcCpuIntrTable.nmiIsr = _CSL_intcNmiDummy; _CSL_intcCpuIntrTable.isr4 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr5 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr6 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr7 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr8 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr9 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr10 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr11 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr12 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr13 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr14 = _CSL_intcDispatcher; _CSL_intcCpuIntrTable.isr15 = _CSL_intcDispatcher;
So CSL_intcPlugEventHandler just plug your own ISR in _CSL_intcDispatcher to get second jumping.
However CSL_intcHookIsr will replace the above mapping table in the corresponding place using your "interrupt" function.
CpIntc_dispatchPlug is a BIOS function. BIOS maintains interrupt using its self APIs. In BIOS6 maybe you can mix BIOS APIs and CSL APIs in using interrupt.
Hi River Liu,
Many thanks for replying [with your experiences/expertise]. Let me put more discussion on this [I did some study and went through examples]. Here is my understanding/questions based on what you told. please confirm which is right and which is wrong.
This is the MAJOR diagram
System_Interrupt ==> input event on CICx ==> Host Interrupt ==> eventId[4 to 128] ==> CPUINT[4 to 15]
1. Say, if i don't use any CSL_intcHookIsr, then the default function called for any of the CPUINT4 to CPUINT15 is _CSL_intcDispatcher.
2. Say, if i use CSL_intcHookIsr for say CPUINT 9 and hook MyIsr(), then any Pulse/level sensitive signal on Interrupt PIN 9 will raise/cause the Isr function MyIsr() instead of default _CSL_intcDispatcher.
3. _CSL_intcDispatcher = Function of {CPUINT only}
System_Interrupt ==> input event on CICx ==> Host Interrupt ==> eventId ==> CPUINT
4. CSL_intcPlugEventHandler plugs Isr at event level, say i map event
CSL_intcPlugEventHandler = Function of {evenId, CPUINT}
5. CpIntc_dispatchPlug plugs Isr to the system Interrupt itself.
CpIntc_dispatchPlug = Function of {System_Interrupt}
Hi Team Ti,
Please confirm if my understanding is correct.
Hi,
Anyone member from Ti please respond to my above post
Hi Ti folks,
Still waiting for response :-(, kindly respond
RC Reddy,
I don't know the answer to questions #1-4
As far as #5 is concerned. CpIntc_dispatchPlug simply plugs a table with your function and argument. This table then is used by CpIntc_dispatch when processing CpIntc interrupts.
Hwi_create() - this plugs the interrupt vector and the ISR fxn. When using CpIntc, you must plug the Hwi fxn with CpIntc_dispatch so it knows how to process the CpIntc interrupts.
CpIntc- deals with System interrupts and Host Interrupts.
Hwi - deals with the GEM interrupt contorller.
EventCombiner - deals with the Event Combiner.
Here is a picture, hope this helps:
Judah
If my reply answers your question please mark the thread as answered
Hi Judah,
Thanks for your reply, Also i need answers for questions 1 to 4. I have been re-iterating the same over and over again, please ask any Ti expert [on interrupts ] to clarify/confirm my understanding of the interrupts [questions 1 to 4].
Also why don't Ti publish such a simplified diagrams anywhere in the documents, This simple pic you pasted is worth more than N paragraphs reading and digesting.
Request you to please ask an expert to answer questions on which API at which stage [where my understanding is correct] and also under what situations/contexts, which API is to be used.
Again requesting to you pull in an expert.
Hello RC Reddy,Please see our comments inline confirming your statements. Please let us know if you have any further questions.
Q1: Say, if i don't use any CSL_intcHookIsr, then the default function called for any of the CPUINT4 to CPUINT15 is _CSL_intcDispatcher.A1: That is correct. Here is a snapshot of the _CSL_intcDispatcher function from CSL:interrupt void _CSL_intcDispatcher (void){ Uint32 evtId; Uint32 intrId = (_CSL_intcCpuIntrTable.currentVectId - \ (Uint32)(&_CSL_intcCpuIntrTable) - 4)/4; /* Get the Event Source of the Interrupt */ if (intrId < 8) evtId = CSL_FEXTR(((CSL_IntcRegsOvly)CSL_CGEM0_5_REG_BASE_ADDRESS_REGS)->INTMUX1, \ (intrId-4)*8+6,(intrId-4)*8); else { if (intrId < 12) evtId = CSL_FEXTR(((CSL_IntcRegsOvly)CSL_CGEM0_5_REG_BASE_ADDRESS_REGS)->INTMUX2, \ (intrId-8)*8+6,(intrId-8)*8); else evtId = CSL_FEXTR(((CSL_IntcRegsOvly)CSL_CGEM0_5_REG_BASE_ADDRESS_REGS)->INTMUX3, \ (intrId-12)*8+6,(intrId-12)*8); } if (_CSL_intcEventOffsetMap[evtId] != CSL_INTC_MAPPED_NONE) _CSL_intcEventHandlerRecord[_CSL_intcEventOffsetMap[evtId]].handler ( _CSL_intcEventHandlerRecord[_CSL_intcEventOffsetMap[evtId]].arg ); Q2: Say, if i use CSL_intcHookIsr for say CPUINT 9 and hook MyIsr(), then any Pulse/level sensitive signal on Interrupt PIN 9 will raise/cause the Isr function MyIsr() instead of default _CSL_intcDispatcher.A2: CorrectQ3: _CSL_intcDispatcher = Function of {CPUINT only}System_Interrupt ==> input event on CICx ==> Host Interrupt ==> eventId ==> CPUINTA3: CorrectQ4: CSL_intcPlugEventHandler plugs Isr at event level, say i map event System_Interrupt ==> input event on CICx ==> Host Interrupt ==> eventId ==> CPUINTCSL_intcPlugEventHandler = Function of {eventId, CPUINT}A4: CorrectQ5. CpIntc_dispatchPlug plugs Isr to the system Interrupt itself.System_Interrupt ==> input event on CICx ==> Host Interrupt ==> eventId ==> CPUINTCpIntc_dispatchPlug = Function of {System_Interrupt}A5: Has been explained by Judah
- Uday
--- If you need more help, please reply. If this answers your question, please Verify Answer below this post ---
Hi Uday,
Can you give the code examples for cases 3 to 5? How would you set this up? I am still confused because when I look at some of the code examples, they also mix in BIOS interrupt calls. Is there some advice as to how to seperate the two? Here is an example of two sections of code that I have been trying to compare and understand. They are both in the SRIO example code. It seems like the first interrupt is just set up using BIOS calls and then the other one is linked a few times and then set up in BIOS? Which example above would match each case or are they different from the descriptions above?
Thanks, Brandy
EventCombiner_dispatchPlug (49, (EventCombiner_FuncPtr)Srio_rxCompletionIsr, (UArg)drvHandle, TRUE);
EventCombiner_enableEvent(49);
hSrioCSL = CSL_SRIO_Open (0);
CSL_SRIO_DisableInterruptPacing (hSrioCSL, 0);
CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 0, 0);
CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 1, 0);
CSL_SRIO_RouteLSUInterrupts (hSrioCSL, 2, 0);
CpIntc_dispatchPlug(CSL_INTC0_INTDST0, (CpIntc_FuncPtr)myDioTxCompletionIsr, (UArg)drvHandle, TRUE);
CpIntc_mapSysIntToHostInt(0, CSL_INTC0_INTDST0, 8);
CpIntc_enableHostInt(0, 8);
CpIntc_enableSysInt(0, CSL_INTC0_INTDST0);
eventId = CpIntc_getEventId(8);
EventCombiner_dispatchPlug (eventId, (EventCombiner_FuncPtr)CpIntc_dispatch, 8, TRUE);
Hi Brandy,
good questions you put. even I was preparing the same questions.
Hi Judah and Uday,
Please explain the following in terms of hooking ISR's [again i repeat please tell/explain in context of ISR hooking only]
1. primary v/s secondary interrupts ISR handling?
2. BIOS v/s CSL based ISR handling?
3. when to use CSL functions and when to use BIOS functions?
4. BIOS functions before or after BIOS_start()? [if before or after, what are the consequences]
Primary Interrupts are those that are given a GEM event (There are 128 GEM events). These do not go through INTC. You can hook an ISR for one of these by creating a Hwi instance and specifying the eventId.
Secondary interrupts are those that go through INTC. I think I've already explained that you use CpIntc APIs for configuring this and specifying your ISR handler. Then you create a Hwi that runs the function CpIntc_dispatch() which will determine which Secondary interrupt caused the interrupt and call its ISR handler accordingly.
In BIOS, think of your ISR just like 'C' function. In fact, you would write your ISR as though it was just a regular 'C' function. We save/restore context and determine what cause the interrupt and call the appropriate ISR handler. My recommendation would be if you are using BIOS then use the BIOS ISR handling scheme also.
Use CSL when you need to configure some piece of hardware or writing a driver...like USB, SRIO, or I2C, etc... Use BIOS for thread processing like Hwis (interrupt), Swi, Task.
Before BIOS_start is like the create or setup phase. BIOS_start basically is when things really start working (Interrupts are enabled). You threads will be running, interrupts will be happening, etc...
Brandy,
Here is answer for each of the questions.
In above piece of code, you are configuring interrupts using BIOS APIs only. CSL_SRIO_xxx functions are configuring SRIO there are no BIOS functions for configuring SRIO. CSL_SRIO_xxx functions are not configuring either CICx OR Corepac Intc (so they are not configuring System Interrupt OR Host Interrupt OR EventID OR CPUINT). CSL_SRIO_RouteLSUInterrupts () function is configuring routing ICRR registers to transfer LSUx interrupt (inside SRIO) to INTDSTx (in your case it is INTDST0). INTDST0 is system interrupt to CIC0.
For CSL example about interrupt refer to PDK packages\ti\csl\example\cpintc.
RCReddy,
Here are answers for your queries:
If your application is using SYSBIOS then you should use SYSBIOS Interrupt APIs to configure interrupts. If you are not using SYSBIOS then you should use CSL Interrupt APIs to configure interrupts. If you try to use the both interrupt functions then there will be conflicts in configuring ISTP and so errors in getting interrupts. (Brandy, you already seen this in your previous post about Timer interrupt having problem with NDK).
For answers on questions on 1st and 4th refer to Judah’s reply.
Regards,
Bhavin
Hi Bhavin/Friedland/Judah,
Interrupts being a major part, it comes as a surprise that no keystone training is available, whatever points discussed above can be put in a presentation. I request you to make it simple for the people to understand and also add a keystone training to the same. The bits and pieces information which came out of above discussion can be arranged and put in a document.
We are in process of putting together a Wiki for the interrupts handling. We can certainly put down all above information in that.